AXIS#.MT.VCMD

Description

AXIS#.MT.VCMD returns the derivative of the position loop trajectory (AXIS#.PL.CMD) which is a velocity. AXIS#.MT.VCMD is updated while the drive is in AXIS#.OPMODE 2 and processes the following motion types:

  • Motion tasking
  • Homing
  • Electronic gearing
  • Service motion
  • External trajectory coming from a fieldbus
  • External trajectory calculated from an analog input signal

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

Depends on units. See Velocity Units for details.

Data Type

Float
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
AXIS1.MT.VCMD

50d0h

05h

Signed32

Velocity

-

Read only

No

AXIS2.MT.VCMD

51d0h

05h

Signed32

Velocity

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MT.VCMD

6310

18A6

Signed32

Read Only

Velocity

AXIS2.MT.VCMD

71846

118A

Signed32

Read Only

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.VCMD

6310

Float

Read Only

Velocity

Related Topics

Motion Tasks